Our Brands

Calculating Total Cooling Requirements for Data Centers

White Paper 25     Summary Revision 3     By Neil Rasmussen

This paper describes how to estimate heat output from Information Technology equipment and other devices in a data center such as UPS, for purposes of sizing air conditioning systems. A number of common conversion factors and design guideline values are also included.

Measuring heat output

Heat is energy and is commonly expressed in Joules, BTU, Tons, or Calories.  Common measures of heat output rate for equipment are BTU per hour, Tons per day, and Joules per second. There is no compelling reason why all of these different measures are used to express the same thing.  The mixed use of these measures causes a great deal of confusion. Fortunately, there is a worldwide trend to move all power and cooling capacity measurements to a common standard, the Watt.  For this reason, we will discuss cooling and power capacities in Watts.

The power consumed from the AC power mains is essentially all converted to heat. This fact allows the thermal output of IT equipment in Watts to simply equal its power consumption in Watts. BTU per hour, as is sometimes provided in datasheets, is not necessary in determining the thermal output of equipment. The thermal output is simply the same as the power input except in the case of Voice over IP (VoIP) Routers.

The total heat output of a system is the sum of the heat outputs of the components. The complete system includes the IT equipment, plus other items such as UPS, power distribution, air conditioning units, lighting, and people. Fortunately, the heat output rates of these items can be determined via simple and standardized rules.

A detailed thermal analysis using thermal output data for every item in the data center is possible, but a quick estimate using simple rules gives results that are within the typical margin of error of the more complicated analysis. The quick estimate also has the advantage that it can be performed by anyone without specialized knowledge. A worksheet that allows the rapid calculation of the heat load is provided in the full white paper.

Example of a typical system

The thermal output of a typical system is described. A 5,000 ft2, (465 m2) 250 kW rated data center with 150 racks and a maximum staff of 20 is used as an example. We assume that the data center is loaded to 30% of capacity, which is typical. For a discussion of typical utilization, see White Paper 37, Avoiding Costs from Oversizing Data Center and Network Room Infrastructure. The total IT load of the data center in this case would be 30% of 250 kW, or 75 kW. Under this condition, the total data center thermal output is105 kW, or about 50% more than the IT load. In the typical example, the relative contribution of the various types of items in the data center to the total thermal output is shown in the figure.

Other heat sources

The prior analysis ignores sources of environmental heat such as sunlight through windows and heat conducted in from outside walls. Many small data centers and network rooms do not have walls or windows to the outside, so there is no error resulting from this assumption. However, for large data centers with walls or a roof exposed to the outdoors, additional heat enters the data center which must be removed by the air conditioning system.

Humidification

In addition to removing heat, an air conditioner system for a data center is designed to control humidity. Ideally, when the desired humidity is attained, the system would operate with a constant amount of water in the air and there would be no need for ongoing humidification. Unfortunately, in most air conditioning systems the air-cooling function of the air conditioning system causes significant condensation of water vapor and consequent humidity loss. Therefore, supple-mental humidification is required to maintain the desired humidity level.  For more information on humidification see White Paper 58, Humidification Strategies for Data Centers and Network Rooms.

Sizing air conditioning

Once the cooling requirements are determined, it is possible to size an air conditioning system. The Watt loads of each of the factors described earlier in this summary can be summed to determine the total thermal load. Expressing all measures of power and cooling in Watts simplifies the process. A general rule is that a CRAC system rating must be 1.3 times the anticipated IT load rating plus any capacity added for redundancy. This approach works well with smaller network rooms of under 4,000 ft2 (372 m2).

For larger data centers, the cooling requirements alone are typically not sufficient to select an air conditioner. Typically, the effects of other heat sources such as walls and roof, along with recirculation, are significant and must be examined for a particular installation. The design of the air handling ductwork or raised floor has a significant effect on the overall system performance, and also greatly affects the uniformity of temperature within the data center. The adoption of a simple, standardized, and modular air distribution system architecture, combined with the simple heat load estimation method described, could significantly reduce the engineering requirements for data center design.

For more information on this topic including common conversion factors, design guideline values, and calculation worksheet, please download White Paper 25, Calculating Total Cooling Requirements for Data Centers

Download White Paper 25 Now
Learn more about cooling solutions
Go back to our top White Papers
Browse the entire White Paper Library

Need help?

Support Center

Obtain answers on your own by trying our digital support tools.

Search FAQs

Get answers you need by browsing topic-related Frequently Asked Questions (FAQ).

How to buy?

Easily find the nearest APC Reseller or Distributor in your location.

Find your replacement battery

Find the genuine APC Replacement Battery for your UPS.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.