Server Room and Network Closet - United States

Enter your requirements

User Site Voltage information_stroke

You must select a basic voltage system for the site. Each voltage system consists of a set of voltages as follows:

device_not_commissioned
  • 120 V system is typical of North America and includes 208 V, 240 V, 208 V 3-Phase, and 480 V 3-Phase;
  • device_not_commissioned
  • 230 V system is typical of most of the world and includes 400 V, 400 V 3-Phase;
  • device_not_commissioned
  • 100 V system is typical of Japan and includes 200 V;
  • device_not_commissioned
  • Typical voltage set for Taiwan is 110 V, 220 V 3-Phase, 380 V 3-Phase.
  • 120V (& 208V, 480V) based on your current country selection. To update user site voltage, please change your country

    information_stroke

    Sum of power of all connected devices into the UPS.

      1 20000
      Operating Voltages information_stroke

      You must select a basic voltage system for the site. Each voltage system consists of a set of voltages as follows:

      device_not_commissioned
    • 120 V system is typical of North America and includes 208 V, 240 V, 208 V 3-Phase, and 480 V 3-Phase;
    • device_not_commissioned
    • 230 V system is typical of most of the world and includes 400 V, 400 V 3-Phase;
    • device_not_commissioned
    • 100 V system is typical of Japan and includes 200 V;
    • device_not_commissioned
    • Typical voltage set for Taiwan is 110 V, 220 V 3-Phase, 380 V 3-Phase.
    • Run Time information_stroke

      The amount of minutes / hours on battery that the UPS will keep the connected devices powered up during an electrical outage.

        mins
        information_stroke

        This field represents the amount of oversizing you wish to include in your configuration. For example, if your current configuration adds up to 400 watts of power draw, a 50% oversizing will make sure the recommended units can support your current draw (400 watts) + 50% of this draw (200 watts) for any future expansions.

          0 200
          Rackmountable information_stroke

          Select this to limit search to UPSs that can be mounted within a rack.

            Topology information_stroke

            Describes the architecture/design of the UPS which varies in performance and functionality.

              Continue

              UPS Selector FAQs

              model-img Why does the UPS Selector suggest a longer run time than I have determined from past APC product literature?

              model-img Does the UPS Selector recommend the lowest cost solution?

              model-img How can the UPS Selector say my PC draws 60 Watts when I know it has a 110 Watt power supply in it?

              model-img How does the UPS Selector work?

              model-img What if I want to see more solution options for my system?

              model-img Why does the UPS Selector indicate a lower power rating than the nameplate of my equipment?

              Disclaimer

              The information provided in the APC UPS Selector is provided for general information purposes only. It is subject to change without notice and is provided "as is" without warranty of any kind, express or implied. Different solutions address different needs; please contact an APC sales representative to discuss the best solution for your specific needs.