{}

Vårt varumärke

Sök bland vanliga frågor (FAQ)

Smart-UPS Ultra 5kW Reports "Battery Modules Not Connected" or "Internal RBM Disconnected" Alarm

Issue: The UPS reports "Internal RBM Disconnected" or "Battery Modules Not Connected" alarm on the LCD.

1 2

Product Line: SRTL5KRM2UI, SRTL5KRM2UT

Environment: UPS firmware version 03.1 or earlier

Resolution: This issue is addressed in UPS firmware version 03.2 Upgrade the UPS firmware to version 03.2 or later. Refer to FA170679 or FAQ000242942 for more information on how to update the UPS firmware.

APC Sweden

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj