Search FAQs
SSH script fails to run from PowerChute Network Shutdown with error (java.nio.charset.MalformedInputException: Input length = 1)
Issue:
Configured PowerChute Network Shutdown to run an SSH script and it fails to run and records error (java.nio.charset.MalformedInputException: Input length = 1).
Product:
PowerChute Network Shutdown version 4.3, 4.4, 4.4.1
Environment:
All support Windows OS
Cause:
Wrong encoding select for the script text file.
Solution:
PowerChute Network Shutdown will support text file encoding UTF-8. Save the text file with the required encoding, and PowerChute will trigger it.
Configured PowerChute Network Shutdown to run an SSH script and it fails to run and records error (java.nio.charset.MalformedInputException: Input length = 1).
Product:
PowerChute Network Shutdown version 4.3, 4.4, 4.4.1
Environment:
All support Windows OS
Cause:
Wrong encoding select for the script text file.
Solution:
PowerChute Network Shutdown will support text file encoding UTF-8. Save the text file with the required encoding, and PowerChute will trigger it.
Released for:APC Saudi Arabia
Explore more
Range:
Explore more
Range: