Search FAQs
Where can AR8654 be installed on the NetShelter Networking roof?
Issue:
There are places on the Networking roof where the AR8654 will not install.
Product Line:
NetShelter Networking Cabinets
Environment:
AR3140, AR3340, AR3347 all serial ranges.
Cause:
The Networking roof is different than the standard NetShelter roof.
Resolution:
Please see the attached file for locations where the AR8654 can mount.
There are places on the Networking roof where the AR8654 will not install.
Product Line:
NetShelter Networking Cabinets
Environment:
AR3140, AR3340, AR3347 all serial ranges.
Cause:
The Networking roof is different than the standard NetShelter roof.
Resolution:
Please see the attached file for locations where the AR8654 can mount.
Released for:APC Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: