{}

Our Brands

Search FAQs

Nutanix AHV: Prioritized VMs with 0 second Startup Duration are powered on

Issue:
When a UPS critical event is cleared and PowerChute starts powering on VMs, any prioritized VMs with a 0 second Startup Duration are initially skipped and later powered on.

Product Line:
PowerChute Network Shutdown v4.3, v4.4

Environment:
PowerChute Network Shutdown configured with Nutanix Acropolis Hypervisor (AHV) support


Solution:
This issue will be resolved in the next release of PowerChute Network Shutdown.

Alternatively, if your PowerChute configuration includes priority groups with a 0 second Startup Duration, you can disable VM Startup in PowerChute and power on VMs manually following a shutdown.

APC Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.