{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the weight capacity of NetShelter open frame racks: AR201, AR203A and AR204A?
Issue: 
Static load rating is required. 

Product Line: 
NetShelter Open Frame Racks

Environment: 
All models, all serial numbers. 

Cause: 
On the APC website, weight capacity is not noted in the Specifications tab of the product pages.  

Resolution: 
AR203A and AR204A Weight Capacity 2,000 lb (907.18 kg).  
AR201 Weight Capacity 1,000 lb. (453.6 kg). 

Schneider Electric Saudi Arabia

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.