{}

Our Brands

Search FAQs

What is the Harmonized Tariff Schedule (HTS) or US Tariff Code for NetShelter cabinets?

Issue:
A customer needs the HTS for NetShelter SX, SV or VX cabinets.

Product Line:
NetShelter SX, SV, VX

Environment:
All models, all serial numbers.

Cause:
HTS is needed for export.

Resolution:
Harmonized Tariff Schedule and US Tariff code are the same thing.
The HTS for NetShelter SX, SV and VX is 9403.20.0030.

APC Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.