Search FAQs
Video: How to Configure Alarm Thresholds on your Symmetra PX10-80KVA UPS
Issue:
How to Configure Alarm Thresholds on your Symmetra PX10-80KVA UPS using the integrated PowerView Display
Product line:
Symmetra PX1
Environment:
All Product models, all serial numbers
Cause:
Need for alerts when Load, Redundancy, or Runtime levels exceed predefined limits.
Resolution:
Select the Setup option from the main display
Select Alarms from the setup menu
The threshold you are setting is the minimum acceptable range. Changes are implemented immediately.
Hit escape to return to previous menu.
The following video demonstrates this procedure:
How to Configure Alarm Thresholds on your Symmetra PX10-80KVA UPS using the integrated PowerView Display
Product line:
Symmetra PX1
Environment:
All Product models, all serial numbers
Cause:
Need for alerts when Load, Redundancy, or Runtime levels exceed predefined limits.
Resolution:
Select the Setup option from the main display
Select Alarms from the setup menu
The threshold you are setting is the minimum acceptable range. Changes are implemented immediately.
Hit escape to return to previous menu.
The following video demonstrates this procedure:
Released for:APC Saudi Arabia
Explore more
Range:
Explore more
Range: