{}

Our Brands

Search FAQs

Why does uninstall script for PowerChute Network Shutdown 4.2+ not properly clean up firewalld on RHEL 7.3+ and CentOS 7.3+?

Issue:
uninstall script for PowerChute Network Shutdown 4.2 and above does not properly clean up firewalld on RHEL 7.3 and above and CentOS 7.3 and above.

Product:
PowerChute Network Shutdown version 4.2, and above

Environment:
RHEL 7.3 and CentOS 7.3

Cause:
From RHEL 7.3 release notes, firewalld packages have been upgraded to provide some enhancements over its previous version. Which includes changes in the firewall-cmd, firewall-offline-cmd, firewall-config, and firewall-applet.

Solution:
After running the PowerChute uninstall script run the command

firewall-cmd --remove-service=pcns --permanent

APC Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.