Search FAQs
Do the VED kits fit onto the roofs of the Symmetra UPS?
Issue:
A customer may want to add a VED Kit to a Symmetra UPS.
Product Line:
Network Air and Symmetra
Environment:
All versions and serial ranges.
Cause:
A customer may want to provide cooling to a Symmetra that's installed in a row of cabinets by utilizing Vertical Exhaust Duct Kits.
Resolution:
The VED kits are not compatible with the Symmetra roof design.
A customer may want to add a VED Kit to a Symmetra UPS.
Product Line:
Network Air and Symmetra
Environment:
All versions and serial ranges.
Cause:
A customer may want to provide cooling to a Symmetra that's installed in a row of cabinets by utilizing Vertical Exhaust Duct Kits.
Resolution:
The VED kits are not compatible with the Symmetra roof design.
Released for:APC Saudi Arabia
Explore more
Range:
Explore more
Range: