Search FAQs
NetBotz 200 | Downloads & Documentation
NOTICE! |
---|
The NetBotz 200 is End-of-Support. See NetBotz | End of Sale & End of Support Information for additional details. |
Issue:
Downloads and Documenation for the NetBotz rack monitor 200.
Product Line:
NetBotz Rack Monitor 200
Environment:
Netbotz 200 (all firmware versions)
Cause:
The NetBotz 200 is no longer supported as of October 2018. The available downloads and documentation can be found below.
Resolution:
Attached are the most recent copies of the following:
- Installation and Quick Configuration Manual
- User's Guide
- Firmware: apc_hw03_aos390_nb200375.exe
- Release Notes
- Modbus Register Map
Released for:APC Saudi Arabia
Attachment(s)
Explore more
Product:
Explore more
Product: