Search FAQs
What is the minimum and maximum mounting depth for the SYAOPT1, and does it fit into the NetShelter 4-post rack?
Issue:
Customers may want to make sure the SYAOPT1 will mount into a particular cabinet, especially our 4-post racks.
Product Line:
Symmetra 4-Post Rack Mounting Rails SYAOPT1
Environment:
All serial ranges.
Cause:
Customers want to make sure the Symmetra 4-post rails will mount into their rack.
Resolution:
Yes, the SYAOPT1 will mount into both the NetShelter AR203A and AR204A. They are 29.42" (747mm) deep.
Minimum Mounting Depth: 27.5" (698.5mm)
Maximum Mounting Depth: 34.5" (876.3mm)
Customers may want to make sure the SYAOPT1 will mount into a particular cabinet, especially our 4-post racks.
Product Line:
Symmetra 4-Post Rack Mounting Rails SYAOPT1
Environment:
All serial ranges.
Cause:
Customers want to make sure the Symmetra 4-post rails will mount into their rack.
Resolution:
Yes, the SYAOPT1 will mount into both the NetShelter AR203A and AR204A. They are 29.42" (747mm) deep.
Minimum Mounting Depth: 27.5" (698.5mm)
Maximum Mounting Depth: 34.5" (876.3mm)
Released for:APC Saudi Arabia
Explore more
Range:
Explore more
Range: