Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Is the ACSC fan system fault tolerant?
Issue:
Is the ACSC fan system fault tolerant? 
 
Product line:
ACSC100, ACSC101
 
Environment:
InRow Cooling
 
Cause:
 
Resolution:
Yes, there are 2 power supplies in the unit for the condenser and evaporator fans. If 1 fails the other can supply 70% of the maximum power needed, so maximum fan capacity would be reduced approximately 30%. A user can replace the failed power supply from the front of the unit while the ACSC is still in operation. The evaporator fans are also hot swappable.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.