{}

Our Brands

Search FAQs

Uniflair SNMP (Simple Network Management Protocol)

Issue:
This dcoument describes the Uniflair SNMP (SimpleNetwork Management Protocol).

Product line:
Uniflair

Environment:
All Models and Serial Numbers

Cause:
Install

Resolution:

Simple Network Management Protocol

Simple Network Management Protocol

Simple Network Management Protocol

The units, all equipped with an apposite RS485 card, are connected with each other using a serial cable RS485. The last unit is connected to the resistor, the first unit is connected to the Webgate, which is the interface to the ethernet company line, where there is the supervisory software (SNMP manager).

Necessary Material:

• 1 webgate every 16 units webgate

• 1 RS485 serial card for every control; RS485 serial card

• 1 resistor (120 Ω). resistor (120 Ω).

 pCOWeb pCOWeb is a device that permits to connect the units directly to the Ethernet line. This card can be used only on the new units, like Leonardo Evolution or Amico with pCO1. pCOWeb transform the unit in a computer, with its IP number.

INSTALLATION

The operations to follow are the following:

• realize the RS485 net;

• configure each unit (address and speed and protocol);

• configure and install the Webgate; avoid connecting the Webgate to the ethernet net. Before having set

correctly the IP address;

• configure the supervisory software according to the MIB table (list of available variables and

addresses).

APC Saudi Arabia

Explore more
Range:
Uniflair Med/Large Room Cooling
Explore more
Range:
Uniflair Med/Large Room Cooling
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.