{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Load is connected to a SmartUPS, yet reports as 0% on the display or in software.

Issue:

Load is connected to a SmartUPS, yet reports as 0% on the display or in software.

Product Line:

Smart-UPS

Environment:

All models, All Serial Numbers

Cause:

Normal Operation

Resolution:
Smart-UPS products may not report very small loads attached to them. If you increase your load to greater than 10% you will see the load reported properly in Powerchute, your Network Management Card, or LCD display (if so equipped). This is normal behavior from the UPS. As the load increases on the UPS, so will the accuracy of the load reporting.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top