{}

Our Brands

Search FAQs

DCE 7.9.3 Communications to an SNMP version 3 device may fail if new passphrases are used.

Issue:
Communications to an SNMP version 3 device in DCE 7.9.3 may fail if new passphrases are used.

Product Line:
Data Center Expert (DCE)

Environment:
Data Center Expert 7.9.3
Potentially any SNMP version 3 device.

Cause:
If you change the SNMP version 3 passphrases for an SNMP version 3 device that is already discovered in DCE, even if you change the SNMP parameters in DCE, you may lose communications and not regain it.

Similarly, if you discover and delete a device, then try to discover with changed SNMP parameters, the device may not properly discover or communicate.

Resolution:
It has been seen that the SNMP parameters are being held in the SNMP daemon and a reboot of the DCE system will clear the old parameters out.

If you have changed passphrases on a device and lost communications within DCE even after updating the passphrases there to, a simple reboot of the DCE server should resolve the communications issue.

This issue should be resolved in an up coming revision of Data Center Expert

APC Nigeria

Explore more
Range:
Data Center Expert
Explore more
Range:
Data Center Expert
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.