{}

Our Brands

Search FAQs

Can the new NetShelter SX 12U and 18U cabinets be stacked?

Issue:
A customer is asking if the new short NetShelter SX cabinets can be stacked.

Product Line:
NetShelter SX 12U and 18U

Environment:
All versions and serial ranges.

Cause:
A customer may want to stack these shorter cabinets.

Resolution:

These cabinets were not designed to be stacked, and should never be stacked. These are stand-alone cabinets, not stackable.

APC Nigeria

Explore more
Range:
NetShelter SX Enclosures
Explore more
Range:
NetShelter SX Enclosures
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.