Search FAQs
Do the NetShelter SX Shock Package cabinets include the OSHPD or IBC High Seismic Area mounting brackets?
Issue:
Preparing for installation, want to know if the pallet brackets from the Shock Packaging can be used to mount the cabinet to the floor.
Product Line:
NetShelter SX Shock Package
Environment:
All versions and serial ranges.
Cause:
Pallet brackets from non-SP cabinet can be used as bolt-down brackets.
Resolution:
The Shock Package cabinets do not include the seismic mounting brackets. They must be purchased separately.
Please use AR7701A-S as the seismic mounting brackets for NetShelter SX SP-series cabinets into IBC High Seismic Area or OSHPD installatiions.
For installation in IBC Low Seismic Area or Moderate Seismic Area please use either AR7701A-S or AR7701.
Preparing for installation, want to know if the pallet brackets from the Shock Packaging can be used to mount the cabinet to the floor.
Product Line:
NetShelter SX Shock Package
Environment:
All versions and serial ranges.
Cause:
Pallet brackets from non-SP cabinet can be used as bolt-down brackets.
Resolution:
The Shock Package cabinets do not include the seismic mounting brackets. They must be purchased separately.
Please use AR7701A-S as the seismic mounting brackets for NetShelter SX SP-series cabinets into IBC High Seismic Area or OSHPD installatiions.
For installation in IBC Low Seismic Area or Moderate Seismic Area please use either AR7701A-S or AR7701.
Released for:APC Nigeria
Explore more
Range:
Explore more
Range: