Search FAQs
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (NBPD0180) ?
The NetBotz Wireless Sensor Pod 180 (NBPD0180) supports the following sensors:
Warning: Only the sensors listed above are compatible with the NBPD0180. Other sensors will not function and will damage the device.
Sensor Name | APC/NetBotz Part Number |
---|---|
NetBotz Door Switch Sensor for APC Racks - 12 ft | NBES0303 |
NetBotz Door Switch Sensor for APC Racks - 62 in | NBES0313 |
NetBotz Door Switch Sensor for Third Party Racks - 62 in | NBES0312 |
NetBotz Door Switch Sensor for Rooms or Third Part Racks - 50 ft | NBES0302 |
APC Temperature Sensor - 13 ft | AP9335T |
APC Temperature & Humidity Sensor - 13 ft (Only reports temperature when connected to the NBPD0180 | AP9335TH |
NetBotz Temperature Sensor - 32 in | NBES0311 |
NetBotz Dry Contact Cable (Requires BotzWare 4.5.0) | NBES0304 |
Warning: Only the sensors listed above are compatible with the NBPD0180. Other sensors will not function and will damage the device.
Released for:APC Nigeria
Explore more
Range:
Explore more
Range: