FAQを参照する
Why does my Smart UPS Modular Ultra show "Unknown UPS internal error [3B7D-00A0]" on the display?
Issue:
Product Line:
Environment:
Resolution:
This specific message occurs when the Redundant Intelligence Module (RIM) is initializing after power up. In later versions of the NMC/Display firmware, the messaging is changed to "RIM initializing, Do not remove MIM". Please upgrade the NMC/Display firmware to SUCAN 2.5.1.3 to see update messaging. You can upgrade the firmware by following this FAQ: https://www.apc.com/jp/ja/faqs/FAQ000261841/
After performing a UPS Firmware upgrade, removing and installing the Intelligence Modules, or when the UPS is booting up from a brains dead, you may see the display show "Unknown UPS internal error [3B7D-00A0]".
Product Line:
Smart UPS Modular Ultra
Environment:
All models, all serial numbers
Resolution:
This specific message occurs when the Redundant Intelligence Module (RIM) is initializing after power up. In later versions of the NMC/Display firmware, the messaging is changed to "RIM initializing, Do not remove MIM". Please upgrade the NMC/Display firmware to SUCAN 2.5.1.3 to see update messaging. You can upgrade the firmware by following this FAQ: https://www.apc.com/jp/ja/faqs/FAQ000261841/
公開先:APC 日本
詳細を見る
製品:
詳細を見る
製品: