FAQを参照する
Smart UPS Modular Ultra A7A1 Power Module Error
Product Line:
Environment:
Resolution:
NMC/Display Firmware - https://www.apc.com/jp/ja/faqs/FAQ000261841/
UPS Firmware - https://www.apc.com/jp/ja/faqs/FAQ000261838/
Different ways to Upgrade UPS Firmware - https://www.apc.com/jp/ja/faqs/FA164737/
Smart UPS Modular Ultra
Environment:
All models, all serial numbers
Resolution:
If you see an “A7A1” error on a Power Module, please do not replace the Power Module in question. This error code occurs when there is a PM with firmware 3.3 (or later) and it cannot get an appropriate response from the IM running with UPS firmware 10.8. To fix this issue, please upgrade the UPS to 13.2 (or later). Please follow the process below to upgrade the Firmware.
If the issue persists after upgrading the firmware, please get the Power Module replaced.
NMC/Display Firmware - https://www.apc.com/jp/ja/faqs/FAQ000261841/
UPS Firmware - https://www.apc.com/jp/ja/faqs/FAQ000261838/
Different ways to Upgrade UPS Firmware - https://www.apc.com/jp/ja/faqs/FA164737/
公開先:APC 日本
詳細を見る
製品:
詳細を見る
製品: