FAQを参照する
Easy UPS Online software (Schneider UPS/APC UPS) has been discontinued
Product Line:
Schneider UPS Software
Environment:
Any SRV UPS with APV9601/ APVS9601 installed using Schneider UPS software
Cause:
APV9601/ APVS9601 is discontinued.
Resolution:
The Easy UPS Online SNMP Cards (APV9601, APVS9601) are discontinued as of 31st Aug 2023.
In line with the SNMP Cards, the Easy UPS Online Software & the Shutdown Wizard are discontinued too. Please note that SRV UPS are supported with PowerChute Serial Shutdown for Serial/USB communication and AP9544 along with PowerChute Network Shutdown for network communication, hence there's no dependency on this software.
If the users wish to continue using their APV9601/APVS9601 and needs to use the associated UPS monitoring software &/or shutdown wizard, they can be downloaded from this FAQ. This FAQ will also be updated to continue supporting our existing customers, as security updates will also be published through this article.
The firmware update file for APV9601/APVS9601 is also available in this article for download.