Search FAQs
What is green mode in Easy UPS SRV3KUXI-IN?
Green Mode:
1. An illuminated leaf icon indicates that the unit is working in Green mode.
2. When this mode is enabled, connected equipment receives utility input power through the bypass relay as long as input voltage and frequency are within the configured limits.
3. If utility power goes out of range, the load is transferred to online mode. The power to the connected equipment may be interrupted for up to 10 milliseconds.
1. An illuminated leaf icon indicates that the unit is working in Green mode.
2. When this mode is enabled, connected equipment receives utility input power through the bypass relay as long as input voltage and frequency are within the configured limits.
3. If utility power goes out of range, the load is transferred to online mode. The power to the connected equipment may be interrupted for up to 10 milliseconds.
Released for:APC India
Explore more
Product:
Explore more
Product: