Search FAQs
How to enable manual bypass mode in SRV3KUXI-IN through the display?
Follow the below steps to enable the bypass operation manually:
1. Press enter key for the main menu option.
2. Select 'byp' option from the main menu using navigation keys.
3. Select the option "PUT" to enter the UPS into the bypass operation manually.
4. Bypass symbol will indicate on the right side of the display to confirm that the UPS is in bypass mode.
1. Press enter key for the main menu option.
2. Select 'byp' option from the main menu using navigation keys.
3. Select the option "PUT" to enter the UPS into the bypass operation manually.
4. Bypass symbol will indicate on the right side of the display to confirm that the UPS is in bypass mode.
Released for:APC India
Explore more
Product:
Explore more
Product: