{}

Our Brands

Search FAQs

UPS BVX2200LI-IN showing red led with constant tone ?

Possible Cause:  Occurrence of an overload condition.
Solution:1)The power being used by the connected equipment has exceeded the capacity of the unit.
2)Unplug devices connected to UPS output socket one at a time to remove overload.
Note: If the detected problem is not corrected, contact Schneider Electric customer care.

APC India

Explore more
Product:
BVX2200LI-IN
Explore more
Product:
BVX2200LI-IN
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.