Search FAQs
UPS BVX1200LI-IN showing red led with constant tone ?
Possible Cause: Occurrence of an overload condition.
Solution:1)The power being used by the connected equipment has exceeded the capacity of the unit.
2)Unplug devices connected to UPS output socket one at a time to remove overload.
Note: If the detected problem is not corrected, contact Schneider Electric customer care.
Solution:1)The power being used by the connected equipment has exceeded the capacity of the unit.
2)Unplug devices connected to UPS output socket one at a time to remove overload.
Note: If the detected problem is not corrected, contact Schneider Electric customer care.
Released for:APC India
Explore more
Product:
Explore more
Product: