Benefits of Our Trade-UPS Program
The APC Trade-UPS program is a cost-effective way to upgrade your existing units and protect your latest investment. Trade in any UPS, regardless of its manufacturer or its working condition, for the latest APC UPS technology and receive discount on your new purchase
- Discount on APC accessories
As a benefit to our customers, now you can also buy additional APC accessories at a significant discount, if purchased along with your Trade-UPS. - Upgrade to two times the VA of your current UPS capacity
Trade in up to 2X the VA of your current UPS capacity. - Free pick up of existing units
Order new units today and receive free pick up of your retired units back to APC. APC will also pay to have larger UPSs picked up and returned.*
*Applicable only to defined easy access areas - Proper ecological disposal of returned UPSs and batteries for free
All old units, including hazardous UPS batteries, returned to APC will then be properly and ecologically disposed of according to the Government’s Producer Responsibility Scheme on Waste Electrical and Electronic Equipment. - Up to a 3 year factory warranty on new units
Trade-UPS Program Rules
To participate in the Trade-UPS program, the customer must agree to the following rules
- Trading In a Single UPS
Customers can trade in a UPS, for a new UPS, up to two times the VA rating of the UPS being traded in. (For example, if an customer trades in a 750VA UPS, they can purchase up to a 1500VA UPS under the this program).
IMPORTANT: The VA rating of the UPS to be purchased must equal or exceed the amount of the UPS traded in - Cross-Sell purchases
At time of Trade-UPS purchase, customer can purchase a maximum of five additional items at “Trade-UPS/Cross-Sell Pricing”. Additional items can only include Surge products, or UPS accessories relative to the application level of the UPS(s) that are being purchased. Trade-UPS/Cross-Sell purchases are limited to the time of initial Trade-UPS purchase, any additional items purchased after the initial Trade-UPS purchase will not be eligible for the Trade-UPS/Cross-Sell discount.
In the event the UPS being traded in is not returned to APC within 30 days of receipt of the new UPS, the customer shall be charged for the amount of the Trade-UPS/Cross-Sell discount.
APC RESERVES THE RIGHT TO REFUSE ANY TRADEUPS ORDER.
For more information on APC Trade-UPS Program, contact us at Tel: (852) 2579 9699 and our sales representatives will assist you.