Search FAQs
What is the Harmonized Tariff Schedule (HTS) or US Tariff Code for NetShelter cabinets?
Issue:
A customer needs the HTS for NetShelter SX, SV or VX cabinets.
Product Line:
NetShelter SX, SV, VX
Environment:
All models, all serial numbers.
Cause:
HTS is needed for export.
Resolution:
Harmonized Tariff Schedule and US Tariff code are the same thing.
The HTS for NetShelter SX, SV and VX is 9403.20.0030.
A customer needs the HTS for NetShelter SX, SV or VX cabinets.
Product Line:
NetShelter SX, SV, VX
Environment:
All models, all serial numbers.
Cause:
HTS is needed for export.
Resolution:
Harmonized Tariff Schedule and US Tariff code are the same thing.
The HTS for NetShelter SX, SV and VX is 9403.20.0030.
Released for:APC Egypt
Explore more
Range:
Explore more
Range: