{}

Our Brands

Search FAQs

What solution does APC recommend for protecting a VDSL data-line?

The PNETR6 and the PNET1GB are compatible with the associated data rates of VDSL and connection of most modems. For applications requiring data line surge suppression for VDSL networks, either of these two models should be recommended, depending whether the application requires rack-mount or standalone installation.

APC Egypt

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.