{}

Our Brands

Search FAQs

How many bonding points are on the NetShelter SX cabinet and where are they located? What are the dimensions of the holes?

Issue:
Installation requires the number of bonding points, their location, size and dimensions.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Cabinets need to be bonded to a common ground.

Resolution:
See attached file

APC Egypt

Attachment(s)

20140710 NetShelter SX Bonding Points Rev2..pdf20140710 NetShelter SX Bonding Points Rev2..pdf [431.34 KB]
Explore more
Range:
NetShelter SX EnclosuresNetShelter Specialty Enclosures
Explore more
Range:
NetShelter SX EnclosuresNetShelter Specialty Enclosures
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.