Consulter notre FAQ
Improper Neutralization of Input During Web Page Generation ('Cross-site Scripting') vulnerability (NMC3 RPDU2G)
Issue:
CWE-79: Improper Neutralization of Input During Web Page Generation ('Cross-site Scripting') vulnerability exists when an outlet user can create a “outlet link” which could allow the security token for a superuser to be forwarded to a machine controlled by the attacker, allowing the user to access the system with elevated privileges. Specifying all links as no referrer blocks the security token from being sent.
Product Lines:
Solution:
A firmware update has been made available to address CWE-79, and has been attached to this article. Please use the below chart to select the proper firmware version.
CWE-79: Improper Neutralization of Input During Web Page Generation ('Cross-site Scripting') vulnerability exists when an outlet user can create a “outlet link” which could allow the security token for a superuser to be forwarded to a machine controlled by the attacker, allowing the user to access the system with elevated privileges. Specifying all links as no referrer blocks the security token from being sent.
Product Lines:
Product | Version |
AP7xxxx and AP8xxx with NMC2 | V6.9.6 or earlier |
AP7xxx and AP8xxx with NMC3 | v1.1.0.3 or earlier |
APDU9xxx with NMC3 | v1.0.0.28 or earlier |
Solution:
A firmware update has been made available to address CWE-79, and has been attached to this article. Please use the below chart to select the proper firmware version.
AP7xxxx and AP8xxx with NMC2 | v7.0.6 of the Rack PDU firmware includes a fix for this vulnerability and is available for download here |
AP7xxx and AP8xxx with NMC3 | v1.2.0.2 of the Rack PDU firmware includes a fix for this vulnerability and is available for download here |
APDU9xxx with NMC3 | v1.2.0.2 of the Rack PDU firmware includes a fix for this vulnerability and is available for download here |
Publié pour:APC Algeria
Pièce(s) jointe(s)
En savoir plus
Gamme :
En savoir plus
Gamme :