Consulter notre FAQ
Modbus support for SMT, SMC, SMTL, SCL Smart Connected UPS
Issue:
What Smart Connected UPS support Modbus communications.
Product Lines:
SMT Smart Connected UPS
SMC Smart Connected UPS
SMTL Smart Connected UPS
SCL Smart Connected UPS
Environment:
Smart Connect UPS connected to local network using the SmartConnect port.
Cause:
Informational
Solution:
SMT Smart Connected UPS with firmware 4.1 or above will communicate via Modbus over Serial and USB.
SMTL Rack Mount Smart Connected UPS models 750 and 1000 will communicate via Modbus over Serial and USB SMTL750RM2UC requires firmware 01.3 SMTL1000RM2UC requires firmware 01.5.
SMTL Rack Mount Smart Connected UPS model 1500 will communicate via Modbus over Serial only.
SMC Smart Connected UPS do not support Modbus communication.
SCL Smart Connected UPS models with an integrated Network Management Card (IE:SCL500RM1UNC) support Modbus over TCP to the card.
NOTE: The SMT and SMTL Smart-UPS with a Network Management Card AP9630, AP9631, AP9635 with firmware 6.4.6 or above supports Modbus over TCP. Smart-UPS with AP9640 and AP9641 support Modbus over TCP.
Links to
What Smart Connected UPS support Modbus communications.
Product Lines:
SMT Smart Connected UPS
SMC Smart Connected UPS
SMTL Smart Connected UPS
SCL Smart Connected UPS
Environment:
Smart Connect UPS connected to local network using the SmartConnect port.
Cause:
Informational
Solution:
SMT Smart Connected UPS with firmware 4.1 or above will communicate via Modbus over Serial and USB.
SMTL Rack Mount Smart Connected UPS models 750 and 1000 will communicate via Modbus over Serial and USB SMTL750RM2UC requires firmware 01.3 SMTL1000RM2UC requires firmware 01.5.
SMTL Rack Mount Smart Connected UPS model 1500 will communicate via Modbus over Serial only.
SMC Smart Connected UPS do not support Modbus communication.
SCL Smart Connected UPS models with an integrated Network Management Card (IE:SCL500RM1UNC) support Modbus over TCP to the card.
NOTE: The SMT and SMTL Smart-UPS with a Network Management Card AP9630, AP9631, AP9635 with firmware 6.4.6 or above supports Modbus over TCP. Smart-UPS with AP9640 and AP9641 support Modbus over TCP.
Links to
Modbus Implementation in APC Smart-UPS
https://www.apc.com/us/en/download/document/SPD_MPAO-98KJ7F_EN/
Modbus Installation and Troubleshooting for AP9635/43/44 Network Management Card
https://www.apc.com/us/en/download/document/SPD_AKAR-8KETBK_EN/
Software interface for Switched Outlet and UPS Management in Smart-UPS
https://www.apc.com/us/en/download/document/SPD_MPAO-99NQL2_EN/
Publié pour:APC Algeria
En savoir plus
Gamme :
En savoir plus
Gamme :