Consulter notre FAQ
How to verify APC UPS is communicating over USB with Mac OS X
Issue:
How to verify APC UPS is communicating over USB with Mac OS X
Product Line:
All USB enabled Smart-UPS and Back-UPS
Environment:
Mac OS X 10.?
Cause:
Informational
Solution:
Open a terminal window on the system and enter the command
system_profiler SPUSBDataType
In the example above there was a Back-UPS BR 700G attached to the system running Mac OS X 10.12.6 via USB.
How to verify APC UPS is communicating over USB with Mac OS X
Product Line:
All USB enabled Smart-UPS and Back-UPS
Environment:
Mac OS X 10.?
Cause:
Informational
Solution:
Open a terminal window on the system and enter the command
system_profiler SPUSBDataType
In the example above there was a Back-UPS BR 700G attached to the system running Mac OS X 10.12.6 via USB.
Publié pour:APC Algeria
En savoir plus
Catégorie :
En savoir plus
Catégorie :