Consulter notre FAQ
Video: How to verify USB device drivers are loaded in Windows OS
Issue:
Need to verify USB device drivers have loaded on Windows OS
NOTE: The USB drivers for communications between APC UPS and Windows OS are pre-installed in the Windows OS.
The drivers should load automatically once the APC UPS has been connected to the computer using the proper USB cable.
If the drivers do not load automatically once the USB cable has been connected to the UPS and the computer, open C:\Windows\System32\drivers and verify that hidclass.sys, hidparse.sys, and hidusb.sys are available.![Screenshot of Windows Device Manager Screenshot of Windows Device Manager](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009o2kFQAQ&oid=00DA0000000abSmMAI)
Once PowerChute has been installed, the driver shown under Device Manager - Batteries will change from HID UPS Battery to APC UPS. If PowerChute has been installed, verify that apcups.inf is available in C:\Windows\System32\DriverStore\FileRepository.
![Image of Windows Device Manager with APC UPS Battery Image of Windows Device Manager with APC UPS Battery](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009o2kGQAQ&oid=00DA0000000abSmMAI)
Products:
PowerChute Personal Edition
PowerChute Business Edition
PowerChute Serial Shutdown
Environment:
Microsoft Windows Vista, 7, 8x, 10, 11
Microsoft Server versions 12,16, 19, 22
Solution:
Go to Control Panel -> Device Manager -> Batteries to view the drivers. There you should see either HID UPS Battery or APC UPS. Also, in Device Manager, go to Human Interface Devices, and there you should see American Power Conversion USB UPS.
If further assistance is required, please see Schneider Electric FAQ Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Need to verify USB device drivers have loaded on Windows OS
NOTE: The USB drivers for communications between APC UPS and Windows OS are pre-installed in the Windows OS.
The drivers should load automatically once the APC UPS has been connected to the computer using the proper USB cable.
If the drivers do not load automatically once the USB cable has been connected to the UPS and the computer, open C:\Windows\System32\drivers and verify that hidclass.sys, hidparse.sys, and hidusb.sys are available.
- hidclass.sys, hidparse.sys, and hidusb.sys are included with the Windows OS. If they are missing from the system, you must install them via the Windows OS install media.
Once PowerChute has been installed, the driver shown under Device Manager - Batteries will change from HID UPS Battery to APC UPS. If PowerChute has been installed, verify that apcups.inf is available in C:\Windows\System32\DriverStore\FileRepository.
Products:
PowerChute Personal Edition
PowerChute Business Edition
PowerChute Serial Shutdown
Environment:
Microsoft Windows Vista, 7, 8x, 10, 11
Microsoft Server versions 12,16, 19, 22
Solution:
Go to Control Panel -> Device Manager -> Batteries to view the drivers. There you should see either HID UPS Battery or APC UPS. Also, in Device Manager, go to Human Interface Devices, and there you should see American Power Conversion USB UPS.
If further assistance is required, please see Schneider Electric FAQ Video: Troubleshooting no communication between UPS and PowerChute Business Edition
Publié pour:APC Algeria
En savoir plus
Gamme :
En savoir plus
Gamme :