Consulter notre FAQ
Can the NetShelter CX be locked?
Issue:
The NetShelter CX needs to be locked
Product Line:
NetShelter CX
Environment:
All versions and serial numbers.
Cause:
Make sure that no unauthorized persons can access the cabinet.
Resolution:
The NetShelter CX AR4018A, AR4018IA, AR4024A, AR4024IA, AR4038A, AR4038IA are fitted with a key lock which secures the front doors and side panels. The rear fan units can be locked using a thumb screw from inside the cabinet.
The CX Mini AR4000MV also has a key lock securing the rear access panel.
The NetShelter CX needs to be locked
Product Line:
NetShelter CX
Environment:
All versions and serial numbers.
Cause:
Make sure that no unauthorized persons can access the cabinet.
Resolution:
The NetShelter CX AR4018A, AR4018IA, AR4024A, AR4024IA, AR4038A, AR4038IA are fitted with a key lock which secures the front doors and side panels. The rear fan units can be locked using a thumb screw from inside the cabinet.
The CX Mini AR4000MV also has a key lock securing the rear access panel.
Publié pour:APC Algeria
En savoir plus
Gamme :
En savoir plus
Gamme :