{}

Our Brands

Search FAQs

Can the NetShelter CX be locked?

Issue:
The NetShelter CX needs to be locked

Product Line:
NetShelter CX

Environment:
All versions and serial numbers.

Cause:
Make sure that no unauthorized persons can access the cabinet.

Resolution:
The NetShelter CX AR4018A, AR4018IA, AR4024A, AR4024IA, AR4038A, AR4038IA are fitted with a key lock which secures the front doors and side panels. The rear fan units can be locked using a thumb screw from inside the cabinet.
The CX Mini AR4000MV also has a key lock securing the rear access panel.

APC Denmark

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.