{}

Unsere Marken

FAQs durchsuchen

Can vertical cable managers be installed inside of the finger style cable managers, like AR7580A, AR7585 or AR7588? If so, what options are there?

Issue:
A customer want to install secondary cable management inside of the vertical cable management fingers.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
Customers may wish to manage cables inside of the finger style cable managers.

Resolution:

See attached file

APC Switzerland

Anlage(n)

20180509 Installing Cable Management Inside of Finger Style Cable Managers Rev 1.pdf20180509 Installing Cable Management Inside of Finger Style Cable Managers Rev 1.pdf [147.06 KB]
Weitere Produktinformationen
Bereich:
Weitere Produktinformationen
Bereich: