FAQs durchsuchen
Video: How to Configure TCP/IP settings on a Symmetra PX10-80 Display
Issue:
Setting up the network management card of the Symmetra PX1 via the PowerView display.
Product line:
Symmetra PX1
Environment:
All Product models, all serial numbers
Cause:
Need to configure IP Address, Subnet Mask, and Gateway for remotely managing the UPS
Resolution:
The following video demonstrates this procedure:
Setting up the network management card of the Symmetra PX1 via the PowerView display.
Product line:
Symmetra PX1
Environment:
All Product models, all serial numbers
Cause:
Need to configure IP Address, Subnet Mask, and Gateway for remotely managing the UPS
Resolution:
The following video demonstrates this procedure:
Veröffentlicht für:APC Switzerland
Weitere Produktinformationen
Bereich:
Weitere Produktinformationen
Bereich: