FAQs durchsuchen
AP5610, AP5615, and AP5616 KVM Switch LDAP Implementation Example
Issue
I need help setting up LDAP with my AP5610, AP5615, and AP5616 KVM Switch.
Product Line
- KVM Switches
- AP5610
- AP5615
- AP5616
- All firmware versions
- LDAP or LDAPS configured in your environment
Cause
This article is provided as an example LDAP set up.
Resolution
Refer to the PDF attachment in this knowledge base.