{}

Nos marques

Consulter notre FAQ
Smart-UPS On-Line with Li-Ion batteries reports "Error B.08" or inaccurate runtime
Issue: Smart-UPS On-Line with Li-Ion batteries reports "Error B.08", or shows  inaccurate runtime remaining on the UPS LCD display, when XBP48RM2U-LI battery pack is connected.

Error B.08

Product Line: SRTL1000RM4UXLI, SRTL1000RM4UXLI-NC, SRTL1500RM4UXLI, SRTL1500RM4UXLI-NC, SRTL1000RMXLI, SRTL1000RMXLI-NC, SRTL1500RMXLI, SRTL1500RMXLI-NC, SRTL2200RM4UXLI, SRTL2200RM4UXLI-NC, SRTL3000RM4UXLI​​​​​, SRTL3000RM4UXLI-NC, SRTL2200RMXLI, SRTL2200RMXLI-NC, SRTL3000RMXLI, SRTL3000RMXLI-NC

Resolution: This is addressed in UPS firmware version 15.3.

Restart the UPS, then update the UPS firmware to the latest version. Refer to FA16473, FA279197 ​​​​​​​or FA170679 to update the UPS firmware.

APC Canada (French)

En savoir plus
Gamme :
Les articles qui pourraient être utiles
En savoir plus
Gamme :