{}

Nos marques

Consulter notre FAQ
Can AR7580A be installed into the 45U NetShelter SX?
Issue:
We need to determine if the 42U finger-style vertical cable managers will fit into a 45U NetShelter SX cabinet.

Product Line:
NetShelter SX, NetShelter Vertical Cable Management

Environment:
AR7580A, AR3155, AR3355 all serial numbers.

Cause:
Availability issues with AR7585 may create the need to use 42U cable managers.

Resolution:

AR7580A will install into the 45U NetShelter SX cabinet but there will be no cable management fingers U-spaces 1 thru 4.
Mounting it in this manner will allow the thru-holes of the mounting rails and cable managers to align.
Please see the attached document.

APC Canada (French)

Pièce(s) jointe(s)
20180719 Installing AR7580A Into a 45U NetShelter Cabinet.pdf [44.06 KB]
En savoir plus
Gamme :
En savoir plus
Gamme :