{}

Nossas marcas

Pesquisar perguntas frequentes

PowerChute Network Shutdown fails to shut down all hosts in a vSAN Cluster when using Advanced UPS Configuration with FTT Support enabled.

Issue:
PowerChute Network Shutdown does not complete the shutdown sequence for the vSAN hosts when UPS critical events occur on multiple different UPS setups at the same time in an Advanced UPS configuration with FTT support enabled.


Product:
PowerChute Network Shutdown version 4.3

Environment:
PowerChute Network Shutdown installed on Windows OS, configured for Advanced UPS configuration with FTT enabled.

Cause:
Software issue.



Solution:
1. Download the attached pcns_vsan_ftt.zip file.
2. Uncompress the file.
3. Open command prompt as an administrator and stop the PowerChute service net stop pcns1
4. Rename C:\Program Files\APC\PowerChute\group1\comp\pcns.jar to original_pcns.jar
5. Copy the uncompress pcns_vsan_fft.jar file to C:\Program Files\APC\PowerChute\group1\comp and rename it to pcns.jar
6. Start the PowerChute service net start pcns1

APC Brazil

Anexo(s)

pcns_vsan_ftt.zippcns_vsan_ftt.zip [2.38 MB]
Conheça mais
Linha:
Conheça mais
Linha: