{}

Our Brands

Search FAQs
Does the NetShelter WX castor kit AR8359 fit onto the AR106, AR109 or AR112.
Issue:
There doesn't appear to be a castor kit for the 6U, 9U or 12U NetShelter WX cabinets.

Product Line:
NetShelter WX

Environment:
All versions and serial ranges.

Cause:
There is a request to add castors to AR106, AR109, AR112, AR106SH4, AR109SH4, AR112SH4, AR106SH6, AR109SH6, AR112SH6, AR106V or AR106VI.

Resolution:
There is no castor kit for the AR106, AR109 or AR112.
The smallest cabinet that has a castor kit available is the AR100  and AR100HD. They use AR8359 available as a castor kit.

APC Belgium

Articles which might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.