FAQs durchsuchen
How do I start a manual Self-Test on my SCL UPS?
Issue: SCL UPS models do not support starting a manual self-test using the power button located on the front panel of the UPS.
Product Line: SCL500RM1UC, SCL500RMI1UC, SCL500RM1UNC, SCL500RMI1UC
Resolution: SCL UPS models will perform an automatic self-test when the UPS is turned on, and on a bi-weekly schedule.
SCL UPS models SCL500RM1UC and SCL500RMI1UC with SmartConnect support manual self-test issued via PowerChute
SCL UPS models SCL500RM1UNC and SCL500RMI1UNC with embedded NMC support manual self-test issued via PowerChute, or the NMC web interface
Veröffentlicht für:APC Austria
Weitere Produktinformationen
Produkt:
Weitere Produktinformationen
Produkt: