{}

Unsere Marken

FAQs durchsuchen

Can the AR8395 busbar install into a NetShelter SV? The busbar installs at three points, but the cabinet only has two accessory mounting brackets.

Issue:
The AR8395 busbar has three installation points.

Product Line:
NetShelter SV, AR8395

Environment:
All models, all serial numbers.

Cause:
NetShelter SV cabinets ship with two accessory mounting brackets.

Resolution:
The AR8395 busbar is compatible with NetShelter SV cabinets, but it does require an extra accessory bracket (AR824002).
See attached file.

APC Austria

Anlage(n)

20180716 AR8393 Installation into the NetShelter SV.pdf20180716 AR8393 Installation into the NetShelter SV.pdf [31.78 KB]
Weitere Produktinformationen
Bereich:
NetShelter Enclosure ComponentsNetShelter SV EnclosuresNetShelter Shelving & Mounting Accessories
Weitere Produktinformationen
Bereich:
NetShelter Enclosure ComponentsNetShelter SV EnclosuresNetShelter Shelving & Mounting Accessories