FAQs durchsuchen
Smart-UPS VT-Galaxy 3500; Run time below limit, run time threshold alarms
Issue:
Smart-UPS VT-Galaxy 3500; Run time below limit, run time threshold alarms
Product line:
Smart-UPS VT-Galaxy 3500
Environment:
All models, all serial numbers
Cause:
Run time below limit, run time threshold alarms may be seen if the user settable threshold is surpassed. This setting may be adjusted per the customer’s requirements.
Resolution:
Adjust the run time alarm threshold in the display or replace batteries
Display menu; Setup>Alarms>Alarm Thresholds>Run Time
Display menu; Setup>Alarms>Alarm Thresholds>Run Time
Veröffentlicht für:APC Austria
Weitere Produktinformationen
Bereich:
Weitere Produktinformationen
Bereich: