DATA CENTER INROW™ COOLING CONTAINMENT SELECTOR
Go to floor layout choices
Inputs
Constraints
Select the Floor Layout for the New Pod (Required)
5.5
X
(Current selection displayed)
feet
X
Length of X Dimension in Layout Chosen
Units
Preferences
Average Rack Power Density
Low (1-3 kW)
X
Recommended Solution
Number of Rows in Pod
1
2
Number of Racks per Row
Less than 5
5 or more
Priority 1
Priority 2
Priority 3
Capital Cost
X
Efficiency
X
Flexibility
X
* Note - These priorities affect the recommended solution only when prior inputs allow for more than one possible solution
Based on your input and layout choice, a "rack air containment, with front containment" cooling pod solution is recommended. This solution is useful in cases where sound attenuation is required. This type of containment solution can be oriented in any direction since both hot and cold air streams are completely contained.


DATA CENTER INROW COOLING CONTAINMENT SELECTOR


    Legal Information     Privacy Policy       Cookie Notice       Change your cookie settings                                                                                                 © 2023, Schneider Electric