Trade in your old UPS receive up to a 25% discount on your new UPS and accessories
Log in if you are a Reseller to get up to a 35% discount on a new UPS
You can upgrade your power capacity up to 4x the original unit or trade in more UPSs for larger units
Free removal and/or shipping of existing units and proper ecological disposal of returned UPSs and batteries
The APC Trade-UPS program is a cost-effective way to upgrade your existing units and protect your latest investment. Trade in any UPS, regardless of its manufacturer or its working condition, for the latest APC UPS technology and receive up to a 25% discount on your new purchase
As a benefit to our customers, now you can also buy additional APC accessories at a significant discount, if purchased along with your Trade-UPS.
Trade in up to 4X the VA of your current UPS capacity or trade in two UPSs for one larger unit.
Order new units today and receive free return shipping of your retired units back to APC. APC will also pay to have larger UPSs picked up and returned.*
*Applicable only to defined easy access areas
All old units, including hazardous UPS batteries, returned to APC will then be properly and ecologically disposed of according to Environmental Protection Agency standards (a $5 to $500 value depending on the UPS).
To participate in the Trade-UPS program, the customer must agree to the following rules
Customers can trade in a UPS, for a new UPS, up to four times the VA rating of the UPS being traded in. (For example, if an customer trades in a 750VA UPS, they can purchase up to a 3000VA UPS under the this program). IMPORTANT: The VA rating of the UPS to be purchased must equal or exceed the amount of the UPS traded in.
Customers can trade in multiple UPSs for larger UPSs. The VA of the multiple units can be combined, then doubled, to get a maximum VA the customer is eligible to trade up to. Customer cannot trade in UPSs for any single or multiple UPSs of lesser value (VA) than the combined VA of all units traded in.
At time of Trade-UPS purchase, customer can purchase a maximum of five additional items at “Trade-UPS/Cross-Sell Pricing”. Additional items can only include Surge products, or UPS accessories relative to the application level of the UPS(s) that are being purchased. Trade-UPS/Cross-Sell purchases are limited to the time of initial Trade-UPS purchase, any additional items purchased after the initial Trade-UPS purchase will not be eligible for the Trade-UPS/Cross-Sell discount.
In the event the UPS being traded in is not returned to APC within 30 days of receipt of the new UPS, the customer shall be charged for the amount of the Trade-UPS/Cross-Sell discount. The dollar value of the Trade-UPS/Cross-Sell discount shall be calculated as the difference between APC Estimated Resale Price (ERP) at time of purchase, and the Trade-UPS/Cross-Sell Price. Customer must supply credit card at time of initial Trade-UPS purchase. This credit card will be debited for the amount of the discount if unit being traded in, is not sent to APC within 30 days.
APC RESERVES THE RIGHT TO REFUSE ANY TRADEUPS ORDER.