UPS Selector - Canada
Home, Home Office / Entertainment
Sum of power of all connected devices into the UPS.
The amount of minutes / hours on battery that the UPS will keep the connected devices powered up during an electrical outage.
Describes the type of input plug that is on the UPS.
The outlet power connections on the UPS.Some business grade UPS’s may have more than one type of outlet connection type.
Sort by
Best Fit

APC Back-UPS 400VA, 120V, Flexible Mounting, Low Profile, Industrial, 3 NEMA outlets
Total Power Draw: 220W
BV400XU
-
Run Time
91%
Max.Capacity Used
Best Performance

APC Back-UPS ES 425VA, 120V, LAM, 6 NEMA outlets (2 surge), Battery is not user replaceable
Total Power Draw: 255W
BE425M-LM
4 min
Run Time
78%
Max.Capacity Used

APC Back-UPS CS 350VA, 120V, 6 NEMA outlets (4 surge)
Total Power Draw: 210W
BK350
6 min
Run Time
95%
Max.Capacity Used

APC Back-UPS 425VA, 120V, 6 NEMA outlets (2 surge), Battery not user replaceable
Total Power Draw: 255W
BE425M
4 min
Run Time
78%
Max.Capacity Used

APC Back-UPS 450VA, 120V, 6 NEMA outlets (2 surge), Battery is not user replaceable
Total Power Draw: 255W
BN450M
4 min
Run Time
78%
Max.Capacity Used

APC Back-UPS 450VA, 120V, 6 NEMA outlets (2 surge)
Total Power Draw: 255W
BN450M-CA
4 min
Run Time
78%
Max.Capacity Used

APC Back-UPS CS 500VA, 120V, beige, 6 NEMA outlets (3 surge)
Total Power Draw: 300W
BK500
8 min
Run Time
67%
Max.Capacity Used

APC Back-UPS, 500VA, Tower, 120V, 6 NEMA 5-15R Outlets , User Replaceable Battery
Total Power Draw: 300W
BK500BLK
8 min
Run Time
67%
Max.Capacity Used

APC Back-UPS 600VA, 120V, 1 USB charging port, 7 NEMA outlets (2 surge)
Total Power Draw: 330W
BE600M1
8 min
Run Time
61%
Max.Capacity Used

APC Back-UPS ES 550VA, 120V, 8 NEMA outlets (4 surge)
Total Power Draw: 330W
BE550G
9 min
Run Time
61%
Max.Capacity Used